You are here: Graphs Application > Graphing Conic Sections

Graphing Conic Sections

The Graphing view lets you graph and explore linear and conic equations analytically in a two-dimensional coordinate system. You can create and analyse lines, circles, ellipses, parabolas, hyperbolas, and general conic equations.

The entry line makes it easy to enter the equation by displaying a template for the type of equation you choose.

Example: Creating a conic ellipse

1. From the Graph Entry/Edit menu, select Equation > Ellipse, and tap the equation type.

2. Type initial values for the coefficients in the provided spaces. Use the arrow keys to move among the coefficients.

3. Press Enter to graph the equation.

Exploring the sample ellipse

1. Drag the ellipse from its centre to explore the effect of translation on the equation.

2. Use the analysis tools, such as Analyse Graph > Analyse Conics > Foci to further explore the graph.

Note: The type of conic determines which analysis tools you can use. In the case of the ellipse, you can obtain its centre, vertices, foci, axes of symmetry, directrices, eccentricity, and latera recta.

3. To explore translation and dilation interactively, define a conic ellipse that uses variables for the h, k, a, and b coefficients. Insert sliders to vary the parameters.

 

© 2006 - 2016 Texas Instruments Incorporated